The Brands
Building brand was rare in the technical field. However, LAPP focused on the brand right from the very start. When Oskar Lapp invented the first cable with colour-coded wires in 1957, he named this innovative product ÖLFLEX® and in doing so, also created a catchy brand name which has accompanied the product during its great success. Since then, LAPP has carried out a consistent branding policy for each of our product lines.
However, this is driven by more than just the desire to establish an easily recognisable product name. Strong branding gives our customers the peace of mind that each individual component allowed to carry the brand name fulfils the same high expectations. Today, the LAPP brands are some of the best-known in the cable technology field and have earned an outstanding reputation as a reliable brand. All over the world, they stand for the values which we and our customers consider paramount: quality, precision, and reliability.
ÖLFLEX® - Single & Multicore Cable


ÖLFLEX® has become synonymous with power and control cables. Our flexible and oil-resistant cables satisfy the highest demands and can withstand even the very toughest conditions.
UNITRONIC® - Shielded & Unshielded Twisted Pair Cable


Our high-quality UNITRONIC® data network cables and field bus components provide a forward-looking solution for all applications in industrial machinery and plant engineering. From transmission of simple control signals to field bus signals in complex network structures – we offer a dependable cabling and connection solution for almost every situation.
ETHERLINE® - Active Network Components


Our ETHERLINE® branded products open up a secure, fast and reliable path to the future of Ethernet applications. The systems are made up of durable and robust cables and connection components for passive network technology, and deliver an effective solution for almost any application, particularly in an industrial environment.
HITRONIC® - Single Mode & Multimode Fiber Optic Cable


HITRONIC® fibre optic cables make transmitting large data volumes easy: fault free, bug proof and at almost light speed. Even electromagnetic radiation does not interfere with the transmission. The HITRONIC® range includes the ideal solution for indoor or outdoor use, for demanding conditions, and even for use in power chains.
EPIC® - Robust Industrial Connectors


EPIC® industrial connectors can be found everywhere in industrial machinery and plant engineering, for measuring, control and drives. EPIC® is a flexible system of housings, inserts and contacts: all extremely robust, absolutely safe and simplicity itself to assemble.
SKINTOP® - The Handy Cable Glands


Simply feed in the cable and twist. That’s it. Our SKINTOP® cable glands provide secure connections in no time. The universal systems are simple but effective. They secure and centre the cable, hermetically seal it and guarantee optimum strain relief.
SILVYN® - Flexible Cable Conduits


The universal range of SILVYN® protection and guidance systems protect cables effectively against dust, moisture, mechanical, thermal and chemical influences. The versatile SILVYN® CHAIN range of energy supply chains also protects and guides cables in dynamic applications.
FLEXIMARK® - Cable Markers


The requirement: permanent marking. The solution: FLEXIMARK®. These sophisticated systems mean that a clear overview inside a control cabinet is no longer just a pipe dream. From simple labels for manual marking through to electronic markings, the FLEXIMARK® range is guaranteed to be permanent.