TOSIBOX® and LAPP bring together the benefits of IP networking plus remote maintenance with one technology.
Modular, simple and secure, the versatile TOSIBOX® enables a secure IoT infrastructure to be set up within minutes, while allowing the IoT ecosystem to be tailored according to a user’s needs. The highly encrypted VPN connection and secure remote connections driven by TOSIBOX® patented technologies have proven particularly useful, given that the solution is internet connection, operator, and device agnostic.
Driving the two innovation leaders’ collaboration is Tosibox’s belief that it has much to gain from LAPP’s expertise in the industrial automation and communications, as well as its strong regional presence in Asia, to help it reach engineers and technical users in markets where it is not represented.
Asia Pacific VP, Tosibox
Below is a success story of a power plant company in Finland, for which similar solutions may be explored and implemented in the Asia Pacific region.

Resolving Several Challenges for
a Global Boiler & Power Plant Supplier
To facilitate clean energy production via its boiler and power plants for clients located across countries in Europe, Finnish company KPA Unicon had to ensure reliable service from its control room in Finland, and collect real-time data from its systems with a ten-millisecond accuracy. In addition, some of its equipment utilized did not support Layer 3, and thus required a Layer 2 option.
The modular and secure nature of TOSIBOX® IoT connectivity technology happened to meet these challenges. Not only did the solution enable remote monitoring for KPA Unicon’s plants around the world, it also enhanced the network’s security with its simplified structure.
Located at geographically different points, each of KPA Unicon’s plants is secured by TOSIBOX® Lock, and creates the accessibility to employees and other users via TOSIBOX® Keys, as defined by the Central Lock Hub in its Finland data center. TOSIBOX® can also support site-to-site (Layer 2) connections, ensuring compatibility with all industrial automation brands and providers in the market.
Synergizing Data for Greater Possibilities
Over 1.2 million lines are stored every hour by KPA Unicon’s central hub via TOSIBOX®, which is almost 29 million lines per day!
Thanks to real-time data collected from its plants located in different geographic locations around the world, KPA Unicon can now offer remote monitoring and plant communications via remote access for its clients. On top of synergizing data for more insightful prediction, the company can also now explore new service concepts, such as tracking plants’ key performance figures on mobile devices, and the real-time monitoring of its devices’ life cycle and predictive maintenance.
Explore Our Solutions

High-end connectivity device bringing unprecedented possibilities for customers to manage their operations and to build new IoT solutions.
- Up to 50 concurrent VPN connections
- VPN throughput up to 70 Mbit/s
- TOSIBOX® Lock 500i with built-in LTE modem
- TOSIBOX® Lock 500

Following the same look and feel as the award-winning TOSIBOX® Lock 500, the new 200 series provide a secure end-point for any type of operational infrastructure.
- Up to 20 concurrent VPN connections
- VPN throughput up to 30 Mbit/s
- TOSIBOX® Lock 250 with integrated WiFi
- TOSIBOX® Lock 210

Industrial router with firewall and secure Plug & Go™ connectivity. It serves as an endpoint for secure remote connections.
- Up to 10 concurrent VPN connections
- VPN throughput up to 10 Mbit/s

Intelligent cryptoprocessing device that enables a secure connection between your computer and one or more TOSIBOX® Locks, giving you full visibility and control over the network devices connected to the Lock. The Key is fully compatible with all existing TOSIBOX® products.
- TOSIBOX® Key USB - must have at least one for the Master Key
- TOSIBOX® Softkey is a computer software that works as a Sub Key controlled via a physical Master Key

Setting up an OT infrastructure is made even easier with the TOSIBOX® Starter Kits. New updated Guide for Setting Up Secure TOSIBOX® System included with Starter Kits.
- TOSIBOX® 500i Starter Kit - TBKIT500B - Lock 500i APAC + Key + SoftKey + Setup Guide Booklet
- TOSIBOX® 150 Starter Kit - TBKIT150 - Lock 150 + Key + SoftKey + Setup Guide Booklet