Automotive
When it comes to automotive production, nothing is more critical than keeping the operation running at top speed. It is important to provide power, control signal, and data connectivity solutions, that ensure greater operational efficiencies, maximum output, and most importantly peace of mind.


For the automotive and ancillary segment, automation is the greater essential to align the different parallel production divisions towards one final output. Ensuring complete connectivity solution of the industry with different stages of production divisions like
- Press Shop
- Body Shop
- Power Train
- Paint Shop
- Final Assembly
- Utility
LAPP Cable & Connection For Automotive Industry
The wire and cable for automotive and ancillary industry have come a long way, from being a small industry to a substantial one, over a decade. There is a need for consolidation to achieve economies of scale, and bring in technology and quality improvements to the industry. Currently, LAPP provides superior quality cables, industrial connectors, glands, conduits, marking systems, tools & accessories, customized systems, and robotics solutions for the intelligent factory of the future with the challenges fulfilled.
For Example
- Continues flexibility
- Robust and extremely high resistance to torsion and reverse bending
- Oil, chemical resistance and extreme temperature solution
- Application-specific and long-lasting
- Slim in construction and light in weight
- EMC and lossless transmission
- Plug and play / complete connectivity solution
- Composite cable solution (power, control/signal, data, and fibre)
Technological expansion and manufacturing development are here to stay and grow. Henceforth smart cabling solutions (slim and light design) with greater intelligence have to be manufactured, as they are the prime facilitators in achieving the objective of interconnecting intelligent devices with low loss.
Broadly, the cables and wires used in these automated equipment/devices have to be flexible, temperature resistant, chemical & mechanical resistant, weather-resistant, flame retardant, halogen-free, fire survival, etc.
Further, automated systems in the automotive and ancillary industry are capable of working more tirelessly, faster, and more exactly than humans. Robot technology hence is becoming one of the most dynamic areas for development. They are now used in almost all industries since they have become a crucial component for complex production processes due to their superiority.
LAPP has substantial expertise at its disposal, as well as decades of experience in working with customers to develop and bring to fruition solutions in the field of robot applications.
We know that dependability is your number one priority "Every connection, Every time". You could choose any manufacturer, but why would you compromise?
Today’s sophisticated robotics and automation processes demand flexibility and durability, and LAPP products have proven to be more than up to the task at dozens of domestic and international facilities. LAPP products provide optimum performance no matter the temperature extremes or how challenging the environments. And they resist fluids, abrasions, and chemicals often found in production processes. You could pay less, but with LAPP products, you get more. More durability and performance which - in the end - saves you money.
Quality is constantly being ensured in our own highly-modern test centers and internationally unique tests to meet the requirements of the products, applications, and standards. The composition of the group with its own in-house production in the main markets gives our international customers the security of being able to access a large assortment of standard products with the corresponding standards all over the world.
LAPP can fall back on its extensive experience over 50 years of development and manufacturing, and based on this has developed various innovations and a high level of production quality and reliability. Also customized solution without compromising and ready-made products from LAPP Systems for Plug and Play.
Products for Automotive Industry
Flexible Power & Control Cables


Highly Flexilbe Power & Control Cables


Data Cables