Ethernet Communication in the Building or Office 

The building network connects computers, servers and the plant with each other and to the Internet.

Special requirements:

- Copper-based ETHERLINE® LAN cables are used for distances up to 100 m

- Fiber optic cables are used for longer distances for the connection between two buildings or within buildings. Various connectors, such as the SC connector, are used for fiber optic-based data transmission.

- HITRONIC® breakout cables are used for cabling within the building.

- HITRONIC® outdoor cables are used for external cabling and cabling between buildings. The permanently installed cables are connected to splice boxes from the HITRONIC® SBX series.

- HITRONIC® fiber optic patchcords are used at the splice boxes to connect the devices.

- ETHERLINE® LAN cables of category Cat.7 or higher are used for office cabling and are permanently installed in the building.

- The RJ45 connector is used for copper-based data transmission

Products used:

For communication from the main cabinet to the office:

- ETHERLINE® LAN cable

- EPIC® DATA RJ45

For communication in the building:

- HITRONIC® breakout cable

- HITRONIC® SBX industrial splice box

- HITRONIC® patch cable

For communication from the office to the Internet:

- HITRONIC® outdoor cable