Understand Connector Selection To Avoid Downtime
A typical manufacturing plant today will have thousands, or even many thousands, of electrical connections on both fixed equipment and moving machines. And it’s just a matter of time before some of those connections fail or wear out, bringing production machines to a dead stop. One way to minimize this downtime is to “connectorize” power and signal cables.
Multi-conductor cables can often be replaced in just minutes if they have connectors at both ends. Hard-wiring that same cable could take hours.
CONNECTORS PREVENT DOWNTIME
Power and signal disruptions have many mechanical and electrical causes, everything from forklift accidents to over-current conditions. With all the mission-critical electrical connections in a modern plant, downtime from damaged electrical connections is a matter of “when” not “if.” Think of connectors as a low-cost insurance policy against this downtime. While connectors do add a small premium to the initial cost of cabling, they will pay for themselves many times over if they eliminate even a few minutes of downtime on a busy production line.
CONNECTOR SELECTION MADE EASY
For all their downtime-prevention benefits, there is one problem with connectors. Call it “connector confusion.”
There are currently dozens of connector varieties and thousands of individual connectors on the market, and even experienced engineers can find it difficult to select the right connector for the job at hand.
Fortunately, connector confusion can be minimized by gathering information on four key technical factors. This information is readily available to any engineer who has already sized the application’s power or signal cables:
- Number of contacts. It may seem obvious that the number of contacts in the connector should match or exceed the number in the cable. But one common mistake is to miscount by not considering the ground. Cable conductor counts typically include ground while connectors do not.
- Wire gauge (AWG). Cable’s wire gauge needs to be within the allowed range of the connector contacts. In general, screw contacts will accommodate a broader range of wire gauges than comparable crimped contacts.
- Cable outside diameter (OD). This fundamental piece of dimensional information is too often overlooked during the specification process. Forgetting OD can have serious consequences. If the OD of the cable is too small relative to the housing, a poor seal will result, creating a performance issue. If the OD is too big, the cable may not fit in the housing easily or at all, creating a potentially costly installation issue.
- Maximum voltage & current. Always double check to make sure the application’s voltage and current are within the rated capacity of the connector. For safety’s sake, this is the cardinal rule of specifying connectors.
Taken together, these factors determine whether the connector will function as a true extension of a given cable. It’s important to emphasize that all four factors must be taken into consideration. A connector, for instance, may meet the requirements on number of contacts, wire gauge and outside diameter but not satisfy the application’s current or voltage requirements.
The four key connector factors should be thought of as a starting point. They don’t capture the effects of difficult operating environments or unusual electrical requirements. But they will help you quickly narrow down the otherwise overwhelming field of connector products.
EPIC® hood EM distribution blue arrows
A NEW CONNECTOR FOR HARSH OPERATING CONDITIONS
Connectors often have to operate in corrosive, electrically noisy or mechanically challenging environments. Our latest connector housings have been designed to thrive in these environments.
Resists Corrosion. Called EPIC® ULTRA, this new rectangular connector housing features nickel-plated zinc hoods and bases with stainless-steel hardware. Together, these corrosion-resistant materials allow the new housing to survive in applications that that would prove challenging for traditional painted aluminum housings.
These applications include equipment installed in outdoor coastal and off-short settings–such as wind farms, marinas, and amusement parks. EPIC® ULTRA is also intended for use in indoor washdown areas–such as those found in food and beverage plants, wineries and breweries.
Resists Electrical Noise. EPIC® ULTRA features an integrated brush-style cable gland, which provides a fast and easy method to terminate a cable shield with a 360-degree, low resistance contact area. Along with the nickel-plated housing, the SKINTOP® forms a conductive shell–or Faraday cage– around the electrical contacts to virtually eliminate electrical interference.
Resists Mechanical Damage. EPIC® ULTRA’s unique mechanical design improves both sealing and strain relief. For one thing, the connector housing’s built-in cable gland not only improves sealing and strain relief but also speeds assembly and eliminates a possible leakage point. For another,the lip seal between the top and bottom housing components has been recessed so it is totally enclosed by the housing when mated and latched. This design feature protects it from mechanical damage and exposure to UV radiation when installed outdoors.