Renewables - EV Charging
Reshaping the Grid with EVs:
Charging into the
Automotive Future
A more sustainable and resilient energy ecosystem is in sight

40 million of Electric Vehicles (EVs) are already on the roads globally, based on a recent report1. Sales of these cars had experienced a massive 35% increase year-on-year. The transition to EV continues as a major growing trend in terms of electrification and net zero emissions commitments.

Imagine your EV as a mobile power plant, not just drawing energy from the electrical grid but also discharging excess energy back into it.

The next trend in EV charging infrastructure, Vehicle-to-Grid (V2G) technology – a visionary development that is increasingly being implemented, enables EVs to function as 'batteries-on-wheels' during peak demand, thus making it possible for EV owners to play a bigger role in the sustainable energy ecosystem!

Discover the Innovations Behind V2G
At the core of V2G technology lies its potential to transform automobile fleets into versatile, valuable assets that replenishes
the power grid by offering a bi-directional energy flow.
Here's a look at the technologies driving V2G:
1
Bi-directional Charging
Specialised hardware such as bidirectional chargers and inverters are needed for energy to flow both ways between the EV and the grid.
2
Smart Grid Integration
V2G uses advanced communication and control technologies to manage the flow of electricity, for real-time monitoring and control of energy exchange between EVs and the grid.
3
Battery Management Systems (BMS)
Efficient V2G operation relies on dynamic infrastructure to monitor the state of charge, health, and EV batteries performance without compromising battery longevity.
4
Communication Protocols
Standards such as the ISO 15118 “plug and charge” help to streamline the charging procedure between EVs, charging stations, and grid operators.
V2G: The New Key to Energy Transition?
More than a power reserve, V2G brings concrete advantages to the electrification game:
Advancing Grid Stability

V2G can help improve electrical grid stability during peak demand periods by intelligently managing the flow of energy to ensure a reliable power supply.
Renewable Energy Integration

V2G can facilitate the integration of renewable energy sources (e.g. solar and wind power) –which often have fluctuating output – by discharging energy back to the grid when needed.
Reduced Home Energy Bills

EV owners could potentially offset their charging costs or even generate income by selling excess energy back to the grid.
Emergency Power for Blackouts

V2G-equipped EVs can act as backup power sources for homes or even communities, in the event of grid outages.
Connectivity by LAPP:
Transitioning to E-Mobility’s Next Chapter
One day there’s going to be a breakthrough. The more attractive the
charging options are, the more electric mobility will catch on.
-Frank Hubbert, Managing Director, LAPP Mobility

Pilot projects and government initiatives related to EVs have begun in leading early adopters such as The Netherlands, United Kingdom and Germany, while pioneering countries in Asia such as Japan are also actively investigating the long-term feasibility of V2G in supporting renewable energy integration for large-scale adoption.

Fostering opportunities for growth through its reliable suite of connectors and cables, LAPP plays a crucial role in today's upward momentum of EV adoption. From parking lots to power grids, take the leap into an exciting energy future with LAPP – your steadfast partner in sustainable mobility!

ACCESS LATEST INNOVATIONS IN DIRECT CHARGING
FROM THE WORLD OF LAPP
REFERENCE:
Global EV Outlook 2024: Outlook for Electric Mobility, https://www.iea.org/reports/global-ev-outlook-2024

© 2025 LAPP India. All Rights Reserved.

LAPP India