Data Centres

Digitalisation for Mordern Data Centres

Enabling digitalisation with solutions from LAPP

The amount of digital data generated worldwide is growing from year to year. In 2015, for example, the global server stock totaled around 58.8 million units. By 2022, this figure had risen to around 85.6 million. Data centers are playing an increasingly important role in this development as the backbone for the highly available provision of digital services. This raises the question of how the gigantic volumes of data in increasingly complex data centers can be transmitted quickly and reliably – but also how the energy infrastructure between the individual components of the data centers can be guaranteed. As an established system provider, LAPP is in a position to offer comprehensive, high-performance solutions from a single source for the growing requirements resulting from digitalisation - from planning to product selection and just-in-time delivery directly to the construction site.

Connect with us today to get started!

Power your operations with LAPP precision, reliability, and unmatched expertise

We always want to offer the best solution. Our experts are on hand to develop a solution together.  We work with your team to design and deliver to your specific needs.

Find more about our Industrial Communication Solutions

Products for data centres

Product list

Find the right solutions for your project in our broad product portfolio for high-performance and reliable data centres and discover the extensive possibilities with LAPP as your partner.

Contact

Our project business team will be happy to provide you with expert advice on planning and implementing your data centre cabling. Contact us for the best connections in the future.

  • Low-voltage Cable

    Copper 

    • N2XH
    • N2XCH
    • (N)2XH
    • (N)2XCH
    • N2XH-F
    • N2XRH
    • NHXH
    • NXHCH
    • RZ1-k (AS) / RZ1-k (AS+)
    • RV-k
    • XLPE/SWA/LSZH
    • CU Rope

    Standards: IEC 60502.1 / BS 6724 / BS 7846 / VDE0276-604

  • Medium-voltage Cable

    Copper

    • N2XS(F)H
    • N2XS(FL)H
    • (N)2XS(F)H
    • (N)2XS(FL)H
    • N2XS(F)2Y
    • N2XS(FL)2Y
    • XLPE/PVC/AWA/LSZH
    • XLPE/PVC/AWA/PVC

    Aluminum

    • NA2XS(F)H
    • NA2XS(FL)H
    • (N)A2XS(F)H
    • (N)A2XS(FL)H
    • NA2XS(F)2Y
    • NA2XS(FL)2Y
    • (N)A2XS(F)2Y
    • (N)A2XS(FL)2Y

    Standards: IEC 60502-2 / IEC 60228 / HD 620 / BS 7835 / BS 6622 / VDE 0276-620

  • Glass fibre & data Cables

    • UNITRONIC® LiYCY / Li2YCYv(TP)
    • ETHERLINE® LAN 350 Cat.6
    • ETHERLINE® LAN 500 Cat. 6A
    • HITRONIC® BTxK A-DQ(ZN)B2Y
    • HITRONIC® HQW A-DQ(ZN)(SR)2Y

    Standards: IEC 60794-1 / IEC 60793-2 / ISO/IEC 11801 / EN 50173-1

  • Connectors and Cable glands

    • EPIC® POWERLOCK
    • EPIC® MH / Modular system
    • EPIC® DATA RJ45
    • SKINTOP® MS-HF-M SC
    • SKINTOP® MS-HF-M BRUSH
    • SKINTOP® MS-HF-M
    • SKINTOP® ST-HF-M
  • Marking systems & Cable protection

    • FLEXIMARK® wrapping labels LCK
    • FLEXIMARK® FCC
    • FLEXIMARK® FCC
    • SILVYN® RILL PA 6
    • SILVYN® SPLIT PA 6
    • SILVYN® KLICK
  • Control Cables, computer and installation cables, and fire-resistant Cables

    • BS 50288-7  RE-2X(St)H
    • BS 50288-7  RE-2X(St)H PIMF
    • ÖLFLEX® Classic 110 CH  
    • ÖLFLEX® 127 HSLH  
    • NHXMH
    • KNX
    • DALI
    • LiH(St)H FE180/E90
    • JE-H(St)H FE180/E90
  • Grounding

    • H07Z1-K
    • H07ZZ-F
    • 6491B - HO7 Z-R
  • Accessories & tools

    • FLEXIMARK® thermal transfer printer
    • Basic Tie cable ties
    • Ty-Gun ERG cable tie pliers

On the safe side: Norms and standards

Standards provide guidelines for manufacturers, installers and inspectors to ensure that data and electricity flow safely, efficiently and reliably, for example by ensuring that cables and electrical lines meet quality and safety standards. Connection solutions from LAPP comply with these standards. An overview of the key standards.

VDE (Association for Electrical, Electronic & Information Technologies)

 

VDE (Association for Electrical, Electronic & Information Technologies)
 
VDE is a German association that develops standards and guidelines for electrical and electronic products. VDE standards cover various aspects, including safety, performance and installation of cables and electrical lines for power and data connections.

IEC (International Electrotechnical Commission)

 

The global non-profit commission is active in more than 170 countries and develops international standards for electrical engineering, electronics and related technologies – with the aim of ensuring the safety, efficiency, reliability and interoperability of electrical installations in data centers, for example.

BS (British Standards)

 

The national standardization body in Great Britain was the first of its kind in the world. Their standards include guidelines for various aspects of connection technology, which are similar to IEC standards, but may also contain specific requirements for the UK market.

  • What special requirements do cables and wires for data centres have to meet?

    LAPP develops high-quality cables and components for the growing challenges associated with digitalisation, for example. Highly complex data centres in particular require fast and reliable transmission in cables that are metal-free, interference-free and tap-proof. At the same time, fibres, cables and components must be of the highest quality to ensure trouble-free operation. This includes the use of halogen-free, low-smoke and flame-retardant cables. The best conditions for maximum safety in terms of building, property and personal protection in data centres are provided by the consistent use of halogen-free cables with optimised fire behaviour. The safety potential can be increased by using cables with additional insulation or functional integrity.
  • What should you keep in mind when making  your product selection?

    High-quality products and easy assembly are crucial factors when it comes to making a selection. If one cable becomes brittle or malfunctions, it affects all other cables from the same reel. Since new installations and removals can be very expensive, investing in durable and high-quality materials is worthwhile in the long run.
  • When purchasing data and power cables, you should pay attention to the following points:

    Data centres are subject to stringent requirements designed to guarantee increased controlled safety in the event of fire (CPR classification). This also applies to the cabling. Among other things, properties relating to fire spread, heat emission and smoke development are analysed. Cables and accessories must also be halogen-free and have other flame-retardant properties - but at the same time fulfil the high performance and quality requirements.
  • Why LAPP products for data centres?

    We have a broad portfolio that guarantees you complete solutions from a single source - all based on our decades of manufacturing and project expertise. We are constantly developing our products and services. Striving for the greatest possible durability, robustness and extreme flexibility is what drives us. Thanks to special sheath materials, LAPP solutions are flame-retardant and halogen-free, thus reducing the risk of flame propagation, high smoke density and toxic fumes in the event of a fire.

    The transfer of energy and the high resistance heat up cables connectors, the constant change between hot and cold due to heating during operation causes cables and connectors to become brittle. In close co-operation with users, the TÜV and the North American UL approval institute, a large number of tests and performance tests were carried out with our ÖLFLEX® cables and SKINTOP® cable glands. This enables us to guarantee our quality standards. Our products are suitable for use worldwide and, of course, are RoHS-compliant.

    Can't find the right product for your needs? Together, we can develop individual solutions, customized for you. Our experts would be happy to guide you.

    Incidentally: expert knowledge is required not only when selecting the components used, but also for assembling and using the components correctly. We would be glad to assist you on site as well.

    Everything from a single source. With us as your partner from idea to realisation. Our project business team will be happy to advise you on the planning and implementation of the electrical installation for your new data centre.