The fourth industrial revolution has radically transformed our economies and the way we work. On the factory floor and out in the field, disparate devices are now connected and have begun sharing and transmitting information, opening up possibilities in this new dynamic environment.
Yet, risks to network security present a real, pressing threat as entire operations could be compromised by ill-advised practices such as using a shared collective password. In a world that’s increasingly reliant on data and diverse connections, a secure and industry-friendly solution is needed.
Presenting TOSIBOX®
A simple and scalable way to build a secure digital access infrastructure
The purpose-designed TOSIBOX® range presents a seamless solution that can be easily integrated into existing operations. It enables reliable two-way connections and data transfers by instantly creating a fully secure connection between devices, bringing about your private highway through the internet of things.
Innovative Features
Offering useful and intuitive capabilities for the user, TOSIBOX® truly game-changes secure OT networking, remote maintenance and network management.
POINT-TO-POINT CONNECTION
Taking Things One Step Further
Furthering the solution’s efficacy is Tosibox’s strategic partnership with LAPP – which takes the powerhouse collaboration to fruition by bringing customers the connectivity they need minus the complexity.
Globally patented technology for automating remote connectivity and OT networking to devices connected to IIo
Wide portfolio of industrial communication & cabling solutions, powered by UNITRONIC®, ETHERLINE®, HITRONIC® and EPIC®
APAC CSO, LAPP Asia Pacific
Aligning with LAPP’s principle of giving customers what they need, its collaboration with TOSIBOX® as well as an all-round understanding of the industry 4.0 landscape, have helped to guide its customers as they make a transition to smarter operations, while delivering greater value should more superior tailored solutions be required.
Explore Our Solutions
TOSIBOX® Lock
is a router with firewall sharing access to devices. One TOSIBOX® Lock protects all devices behind it. As the company grows, more Locks can be added to various locations.
3806230 - TOSIBOX® LOCK 500i (APAC version w/o PS)
Features
8100592 - TOSIBOX® LOCK 250 (w/o PS)
Features
Features
TOSIBOX® Key
is a dongle used to access the network. In addition to a Master Key, the ecosystem can have several users with more physical keys, mobile app or software licenses.
KEY - TBK2
3806220 - TOSIBOX® KEY
Features
controlled via a physical Master Key
3806246 - START KIT W/ KEY SOFTKEY MOBCL LOCK 500i
Features
- Lock 500i APAC + Key + SoftKey + Setup Guide Booklet
- Lock 150 + Key + SoftKey + Setup Guide Booklet
contact your local LAPP sales representative.